how to build a bin or srec file from the MCXPRESSO IDE

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

how to build a bin or srec file from the MCXPRESSO IDE

ソリューションへジャンプ
520件の閲覧回数
Shreyas_Bhat
Contributor II

hello , i have gone through the settings in the properties but could  not find how to change it .
thank you

タグ(1)
0 件の賞賛
返信
1 解決策
442件の閲覧回数
luis_maravilla
NXP Employee
NXP Employee

Hello

 

To generate the .bin and .s19(SREC) file, you need to build your project and in the project, explorer enter the Debug folder,then right click on the .axf file and in the binary utilities option select "Creare Binary" and "Create S-RECORD".

 

To create the .srec file from MCUXpresso changing post build settings please follow the steps described in the BLEDAUG Chapter 5.11.4 step 4

You can use this link Bluetooth Low Energy Demo Applications User’s Guide.

 

Best Regards

Luis

元の投稿で解決策を見る

2 返答(返信)
443件の閲覧回数
luis_maravilla
NXP Employee
NXP Employee

Hello

 

To generate the .bin and .s19(SREC) file, you need to build your project and in the project, explorer enter the Debug folder,then right click on the .axf file and in the binary utilities option select "Creare Binary" and "Create S-RECORD".

 

To create the .srec file from MCUXpresso changing post build settings please follow the steps described in the BLEDAUG Chapter 5.11.4 step 4

You can use this link Bluetooth Low Energy Demo Applications User’s Guide.

 

Best Regards

Luis

468件の閲覧回数
Shreyas_Bhat
Contributor II

can anyone please tell me how to generate serec and bin file after build

0 件の賞賛
返信