Zigbee: ZPS_tsNwkNib structure related to the Network Layer Information Base

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Zigbee: ZPS_tsNwkNib structure related to the Network Layer Information Base

1,240件の閲覧回数
navdeepsinghgil
Contributor II

Zigbee: I do not see any description of ZPS_tsNwkNib structure related to the Network Layer Information Base (NIB) in the application C code provided with JN-AN-1221. Could you please help?. Also in the AgeChildren.c file there are constants like ZPS_NWK_NT_AP_RELATIONSHIP_CHILD and ZPS_NWK_NT_AP_DEVICE_TYPE_ZED. Where are they defined?

0 件の賞賛
返信
1 返信

1,049件の閲覧回数
finstonian
Contributor II

The constants ZPS_NWK_NT_AP_RELATIONSHIP_CHILD and ZPS_NWK_NT_AP_DEVICE_TYPE_ZED are defined in a file named zps_nwk_nib.h which is located in the C:\NXP\bstudio_nxp\sdk\JN-SW-4168\Components\ZPSNWK\Include folder.