ZigBee 3.0 - connect up to 100 nodes

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

ZigBee 3.0 - connect up to 100 nodes

2,970 次查看
jianalai
Contributor II

We are using ZigBee 3.0 and JN-AN-1229-ZPS-Application-Template. We are having the problem of  the connection for 100 nodes. We are connecting 1 coordinator, 40 routers and 60 end devices. Some of the nodes cannot be controlled like the end device can send the data to coordinator but the coordinator cannot send the data to end device. We are using ZPS_eAplAfUnicastDataReq() to send data. Some of the nodes will became unstable after reboot (Some of the nodes cannot joined back to the network). We have changed the configuration setting for the coordinator and routers as the following.

Maximum Number of Nodes = 120

Mac Table Size = 126

Address Map Table Size = 100

Routing Table Size =120

标记 (1)
0 项奖励
回复
3 回复数

2,365 次查看
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Jia Na Lai,

 The Address Map table and The MAC Address table are fully persisted in EEPROM. Therefore, increasing the size of this table and the address map will impact both RAM.

The Coordinator needs to store routes to all the nodes in the network if it is required to communicate with every node - in this case, the Routing table size should be increased to the size of the network.

Note:The Routing table is not persisted and any increase will therefore only affect RAM usage

Best Regards,

Mario

0 项奖励
回复

2,365 次查看
dheerajsawant
Contributor V

Hi Mario, 

 i want to transfer data from CoOrdinator to Sleeping Device. 

need your help . 

I have transferred data from Sleeping device to Co-Ordinator its work fine.

but i don't know how to send data from Co-ordinator. 

if you have Demo code please share.

Please Awaiting for your Reply

0 项奖励
回复

2,365 次查看
patrick_pan
NXP Employee
NXP Employee

Hi, Dheeraj

According to Zigbee Spec, ZED's parent only buffers message for 7.5s when ZED is sleeping otherwise this message will be dropped. So your ZED node must wakeup and poll its parent within 7.5s periodically. 

B.R

Patrick

0 项奖励
回复