Zephyr NXP Driver Security Support

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Zephyr NXP Driver Security Support

1,310 次查看
Emil_10
Contributor II

Setup
Im developing a wifi app for a FRDM-RW612. I am using Zephyr.

 

Context

After enabling the NXP wifi driver, I successfully connected to a standard home wifi using the security type WIFI_SECURITY_TYPE_PSK.

Now I want to connect to a business network using the protocol "EAP-PEAP/MSCHAPv2" or as Zephyr enumerates it: WIFI_SECURITY_TYPE_EAP_PEAP_MSCHAPV2 This turns out to be quite the problem. After investigating the driver, I discovered that there is no specific check for WIFI_SECURITY_TYPE_EAP_PEAP_MSCHAPV2, though there are many others.

Also, none of the applicable options allow for a "user, password" structure. As I understand it, the driver does not seem to support such wifi authentication at this time, and thus does not support "EAP-PEAP/MSCHAPv2".

 

Questions

What security is supported by the Zephyr NXP wifi driver?
Is there a way to connect using EAP-PEAP/MSCHAPv2 with the nxp zephyr wifi driver?
Does the FRDM-RW612 support EAP-PEAP/MSCHAPv2 if I do not go through Zephyr?

标记 (2)
0 项奖励
回复
5 回复数

1,058 次查看
Emil_10
Contributor II

Quick recap for future readers(31/3/2025):
Does the FRDM-RW612 support EAP-PEAP/MSCHAPv2 if I do not go through Zephyr?
Yes in MCUXpresso SDK 24.12.00 the exaple "wifi_wpa_supplicant" can connect using EAP-PEAP/MSCHAPv2 authentication

标记 (1)
0 项奖励
回复

1,278 次查看
Ricardo_Zamora
NXP TechSupport
NXP TechSupport

Hello,

 

Hope you are doing well. Could you please clarify what application are you using?

What versions are you using?

 

Also, are you following any guide?

 

Regards,

Ricardo

Best Regards,
Ricardo
0 项奖励
回复

1,262 次查看
Emil_10
Contributor II

First of all, thanks for taking the time to help, I appreciate it.

Of course I will try to clarify.

Versions

Im using the zephyr on its current main, which would be version "4.1.99".

The NXP hal used on this version has the hash

9dc7449014a7380355612453b31be479cb3a6833

commit: "HEAD is now at 9dc74490 hal_nxp: Include LP Flexcomm driver using the right Kconfig"

Sample

Here i use sample "samples/net/wifi/apsta_mode". It can be found here:
zephyr/samples/net/wifi/apsta_mode at main · zephyrproject-rtos/zephyr · GitHub

I had to modify it slightly by adding the kconfig "CONFIG_WIFI_NXP". I also updated the example to use my wifi network. I disabled the AP mode as I do not need it.

The example works well with a "standard" home wifi using only password and WPA2-psk security. I can also see on my access point that the RW612 is successfully connected.

However, when I try to connect to an enterprise network with user and password using EAP-PEAP-MSCHAPV2 security, the connection fails. The nxp simply doesn't event try to connect. I also see on the access point that no one has tried to connect. I have configured the connect call as follows:

    sta_config.ssid = (const uint8_t *)WIFI_SSID;
    sta_config.ssid_length = strlen(WIFI_SSID);
    sta_config.eap_identity = WIFI_USERNAME;
    sta_config.eap_id_length = strlen(WIFI_USERNAME);
    sta_config.eap_password = WIFI_PASSWORD;
    sta_config.eap_passwd_length = strlen(WIFI_PASSWORD);
    sta_config.security = WIFI_SECURITY_TYPE_WPA_AUTO_PERSONAL;
    sta_config.channel = WIFI_CHANNEL_ANY;
    sta_config.band = WIFI_FREQ_BAND_2_4_GHZ;

    LOG_INF("Connecting to SSID: %s\n", sta_config.ssid);

    int ret = net_mgmt(NET_REQUEST_WIFI_CONNECT, sta_iface, &sta_config,
               sizeof(struct wifi_connect_req_params));

 

After debbuging i arrived here in the NXP zephyr driver.

zephyr/drivers/wifi/nxp/nxp_wifi_drv.c at main · zephyrproject-rtos/zephyr · GitHub

It seems that the supported security here is limited to:

  • No security.
  • WPA2-PSK security.
  • WPA2-PSK-SHA256 security.
  • WPA3-SAE security.
  • WPA3-SAE security with hash-to-element.
  • WPA3-SAE security with both hunting-and-pecking loop and hash-to-element enabled.
  • WPA/WPA2/WPA3 PSK security.

Full list of types in zephyr is here:
Zephyr API Documentation: Wi-Fi Management

Am i using the wrong wifi driver?

Is there maybe a NXP wifi driver branch in development i can check out?

Is the problem just zephyr-NXP related would it be possible to do with the NXP SDK?

0 项奖励
回复

1,097 次查看
Ricardo_Zamora
NXP TechSupport
NXP TechSupport

Hello,

 

Please find following table with supported features list.

 

Wi-Fi requirements

Is supported in Zephyr 4.1.0 release?

“WIFI_SECURITY_TYPE_EAP_PEAP_MSCHAPV2" security

it is supported in WPA2 mode.(with hostapd)

2,4 & 5 GHz

Yes

TLS 1.2 & TLS 1.3 for WPA 2 & 3 private and enterprise

TLS 1.2 supported.

Currently no Wi-Fi sample app is available with TLS 1.3.  if need to add support of TLS1.3, you need to create CCB for this to support

NTP v 4

SNTP is application layer protocol. if zephyr supports SNTP version 4 then it should work on Wi-Fi interface.

As per  https://docs.zephyrproject.org/latest/connectivity/networking/api/sntp.html, zephyr supports NTP v 4.

IPv6 SLAAC

RW612 Wi-Fi interface supports IPv6 SLAAC as it utilizes the zephyr networking stack, which includes support for IPv6 SLAAC.

 

Overview — Zephyr Project Documentation

Network Stack (TCP/IP, https, DHCP)

RW612 Wi-Fi interface supports TCP/IP, https and DHCP as it utilizes the zephyr networking stack, which includes support for TCP/IP, https, DHCP

 

Regards,

Ricardo

Best Regards,
Ricardo

1,062 次查看
Emil_10
Contributor II

Hello 

Thanks for this info its very helpfull. However could it be that this is not for all boards? 

zephyr

When i try using the RW612 in zephyr this is my result:

Emil_10_0-1743402591332.png

Here i used the "wifi/shell".

NXP MCZXpresso SDK 24.12.0
I know the board can do it and that my net is correctly configured since in the NXP SDK i see:

Emil_10_1-1743402736609.png

So as of now it seems that the RW612 definitely supports the authentication type.

However i am still struggling to reproduce the connection when using the zephyr SDK. Would it be possible to elaborate what you mean by "it is supported in WPA2 mode".
Is there a NXP wpa2 Kconfig or something?

Again thanks for helping me out

0 项奖励
回复