Whether the code of KW38 and KW45 is common

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Whether the code of KW38 and KW45 is common

跳至解决方案
508 次查看
wenjie
Contributor I

I am using KW38 now, and the RAM of KW38 is not enough. As far as I know, many software of KW38 and KW45 are compatible, so whether the program of KW38 can be directly run on KW45? I just want to quickly replace it and test how much memory is needed, and verify how much RAM is needed first

标签 (1)
0 项奖励
回复
1 解答
489 次查看
luis_maravilla
NXP Employee
NXP Employee

Hi

KW38 and KW45 are not pin compatible, there are some differences in Application structure and APIs used for each device. For development using a new board, and in order to avoid any issues related to the software, I would recommend checking on the Bluetooth Low Energy Application Developer’s Guide Chapter 9 to see how this structures are integrated; also, this document describes the most commonly used APIs and provides code examples applicable to KW45.

 

I would recommend using the SDK examples for KW45 as base for developing your application if you are trying to move to KW45.

 

Best Regards

在原帖中查看解决方案

0 项奖励
回复
2 回复数
490 次查看
luis_maravilla
NXP Employee
NXP Employee

Hi

KW38 and KW45 are not pin compatible, there are some differences in Application structure and APIs used for each device. For development using a new board, and in order to avoid any issues related to the software, I would recommend checking on the Bluetooth Low Energy Application Developer’s Guide Chapter 9 to see how this structures are integrated; also, this document describes the most commonly used APIs and provides code examples applicable to KW45.

 

I would recommend using the SDK examples for KW45 as base for developing your application if you are trying to move to KW45.

 

Best Regards

0 项奖励
回复
477 次查看
wenjie
Contributor I
Ok, thank you for your answer
0 项奖励
回复