Where is the Apache_Prod_BringupPORT.eww workspace located ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Where is the Apache_Prod_BringupPORT.eww workspace located ?

ソリューションへジャンプ
2,763件の閲覧回数
jasonchiang
NXP Employee
NXP Employee


Hello Sir,

       I read AN5179 application note. The topic of this application note is MKW40 PHY Test Using DTM. It described that " Open Apache_Prod_BringupPORT.eww workspace in IAR " in section 3.2.1.

Where is the Apache_Prod_BringupPORT.eww workspace located in the Freescale website for downloading ? Kindly need your comment. Thanks !

0 件の賞賛
返信
1 解決策
2,390件の閲覧回数
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,391件の閲覧回数
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 件の賞賛
返信
2,388件の閲覧回数
EarlOrlando
Senior Contributor II

Hello,

Unfortunately, the workspace that you are looking for is not available for download. However, you can use the hci_app project which is available in the Kinetis KW40Z Connectivity Software​. This project is located in the path C:\Freescale\KW40Z_Connectivity_Software_1.0.1\ConnSw\examples\bluetooth\hci_app\frdmkw40z\bare_metal\build\iar\hci_app.eww.

If you have any other doubt please don't hesitate on contact me.

Best regards,

Earl Ramírez.

2,388件の閲覧回数
jasonchiang
NXP Employee
NXP Employee

Hello Earl Ramírez,

    Does this hci_app project can run PHY Test Using DTM for MKW40 ?

0 件の賞賛
返信