Where is the Apache_Prod_BringupPORT.eww workspace located ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Where is the Apache_Prod_BringupPORT.eww workspace located ?

跳至解决方案
2,546 次查看
jasonchiang
NXP Employee
NXP Employee


Hello Sir,

       I read AN5179 application note. The topic of this application note is MKW40 PHY Test Using DTM. It described that " Open Apache_Prod_BringupPORT.eww workspace in IAR " in section 3.2.1.

Where is the Apache_Prod_BringupPORT.eww workspace located in the Freescale website for downloading ? Kindly need your comment. Thanks !

0 项奖励
回复
1 解答
2,173 次查看
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

在原帖中查看解决方案

0 项奖励
回复
3 回复数
2,174 次查看
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 项奖励
回复
2,171 次查看
EarlOrlando
Senior Contributor II

Hello,

Unfortunately, the workspace that you are looking for is not available for download. However, you can use the hci_app project which is available in the Kinetis KW40Z Connectivity Software​. This project is located in the path C:\Freescale\KW40Z_Connectivity_Software_1.0.1\ConnSw\examples\bluetooth\hci_app\frdmkw40z\bare_metal\build\iar\hci_app.eww.

If you have any other doubt please don't hesitate on contact me.

Best regards,

Earl Ramírez.

2,171 次查看
jasonchiang
NXP Employee
NXP Employee

Hello Earl Ramírez,

    Does this hci_app project can run PHY Test Using DTM for MKW40 ?

0 项奖励
回复