Where can I find the actual KW39-38-37 radio certification documents?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Where can I find the actual KW39-38-37 radio certification documents?

2,074件の閲覧回数
mic_ge
Contributor I

FRDM-KW38 platforms have passed the CE RED & FCC radio certification. 

Find below for information the certification documents and test reports. 

For further information on the RF test setup please refer to the corresponding RF report on KW38 Product Summary page and FRDM-KW38 page : FRDM-KW38 RF System Evaluation Report for Bluetooth LE Applications AN12517

According the actual AN12517 the radio tests were performed according to EN 300 328 V2.2.1

ラベル(1)
  • KW

タグ(3)
0 件の賞賛
返信
1 返信

2,057件の閲覧回数
antonioconcio
NXP Employee
NXP Employee

Hi Michael,

You can find them attached at below community post:
KW39-KW38-KW37-Radio-certification-documents 

antonioconcio_0-1648740354269.png

Cheers,
Antonio

 

0 件の賞賛
返信