Using NCJ38A with KW45B41Z-EVK

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Using NCJ38A with KW45B41Z-EVK

685件の閲覧回数
cnew01
Contributor IV

Hello:
I cannot use the secure functions on the NCJ38A development kit. It is plugged in to a KW45B41Z-EVK. I have uploaded the CCC Applet revision 2.3.0 to the applet and I have been trying to use commands on the JCShell. I cannot run any of the demos in the usecases demo (can only switch to I2C Interface and cold reset). I've tried the following commands in JCShell and still run into problems. What should I look into to fix this issue?
cm> /select D040000020435F534341000101
=> 00 A4 04 00 0D D0 40 00 00 20 43 5F 53 43 41 00 ......@.. C_SCA.
01 01 00 ...
(107506 usec [SYS])
<= 5F 06 03 02 03 00 90 00 _.......
Status: No Error
cm>
Try: 'help [topic]', '? [topic]' or 'gui command args'
cm> /send 808000FF *9000
=> 80 80 00 FF ....
(106440 usec [SYS])
<= 6D 00 m.
Status: INS value not supported
jcshell: Response APDU did not match expected value!
expected: *9000
response: 6D00

 

0 件の賞賛
返信
1 返信

653件の閲覧回数
Ricardo_Zamora
NXP TechSupport
NXP TechSupport

Hello,

 

Hope you are doing well. Sorry for the inconvenience this might cause you but the information of this product (NCJ38A) it's under NDA (Non-Disclosure Agreement).

 

Could you please contact one of our distributors available in the Distributor Network|NXP to help you with your request? Or you can contact the person who helped you getting this device.

 

I apologize for the inconveniences this might cause you and you project.

 

Best Regards,

Ricardo

0 件の賞賛
返信