Updating MCXW716C NBU over SWD on a custom board – feasibility & recommended workflow

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Updating MCXW716C NBU over SWD on a custom board – feasibility & recommended workflow

513件の閲覧回数
Brainiac
Contributor II

hello, 

On our custom board the MCXW716C is accessible only through the 10-pin SWD header (SWDIO/SWCLK/nRESET).
Can we update the NBU (radio core firmware) over SWD, or is a UART/USB boot-loader interface mandatory?
If SWD updates are supported, please point me to the recommended tool or application note.

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

503件の閲覧回数
sofiaurueta
NXP Employee
NXP Employee

Hello,

Hope you are doing well.

 

You could follow the method described in AN14397 - Programming the MCXW71 Flash for Application and Radio Firmware via Serial Wire Debug Duri.... This method merges the fuse programming, burning of CM33, and NBU firmware operations to produce a single binary file, and downloads the merged binary file only once through the Serial Wire Debug (SWD).

 

Best Regards,

Ana Sofia.

0 件の賞賛
返信