Timer management in a BLE connection

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Timer management in a BLE connection

2,134件の閲覧回数
nidhintomy
Contributor IV

I have 2 questions related to TimerManager in kw38 ble sample app 'frdmkw38_adv_ext_peripheral_bm'.

1. Sample example uses 'TMR_StartLowPowerTimer' API. What is the context of LowPower in this API name?

2. gTmrApplicationTimers_c flag is defined and set its value to 4 in app_preinclude.h file. Can i change value of this flag? If yes, what is the maximum limit?

Best Regards,
Nidhin

 

ラベル(1)
  • KW

0 件の賞賛
返信
1 返信

2,116件の閲覧回数
EduardoZamora
NXP TechSupport
NXP TechSupport

Hello,

According to the Connectivity Framework Reference Manual (inside KW38 docs folder > docs > wireless > common), TMR_StartLowPowerTimer starts a low-power timer which can operate across all power modes, including low-leakage modes. This timer is necessary because MCU can enter low-power mode if there are only active low-power timers.

Taking a look at TimersManager.h, valid range for gTmrApplicationTimers_c macro should be user defined depending on the timers needed by the application.

Regards,
Eduardo.

0 件の賞賛
返信