SoC/TRx 2.4 GHz for bluetooth and proprietary protocols

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SoC/TRx 2.4 GHz for bluetooth and proprietary protocols

ソリューションへジャンプ
3,916件の閲覧回数
tobiasike
Contributor I

Hi anyone.

I am looking for a hardware plattform (RF-TRx or Sytem on chip) for a bigger project, which can be act as an bluetooth (low energy)  node  -- and on the other hand can be configured to handle a simple proprietary protocoll  (without all  the BT features),  its for compatibility mode.  

both configurations are independent, so the are two different firmwares.

best regards / nice weekend

ラベル(3)
タグ(3)
0 件の賞賛
返信
1 解決策
3,545件の閲覧回数
TudorS_
NXP Employee
NXP Employee

The upcoming Kinetis KW41Z will feature (alongside the Bluetooth LE v4.2 capabilities) a generic FSK mode on top of which any proprietary protocol using FSK modulation in the 2.4 GHz band will be implementable.

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
3,546件の閲覧回数
TudorS_
NXP Employee
NXP Employee

The upcoming Kinetis KW41Z will feature (alongside the Bluetooth LE v4.2 capabilities) a generic FSK mode on top of which any proprietary protocol using FSK modulation in the 2.4 GHz band will be implementable.

0 件の賞賛
返信
3,545件の閲覧回数
tobiasike
Contributor I

Thank you very much,   its what i am looking for.

When the device will be available /released  ?

0 件の賞賛
返信
3,545件の閲覧回数
TudorS_
NXP Employee
NXP Employee

The target is early Q3 2016.

There are however alpha programs you can be part of for early access to the technology. Please contact NXP support for more information.

0 件の賞賛
返信
3,545件の閲覧回数
tobiasike
Contributor I

Thank you --  i pick this information for our hardware selection document.

is there a approx. price for the product available ( @ 1kuint) ?

.. or may there are some distributer having this SoC already inside linecard.

0 件の賞賛
返信