Shell in wireless example

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Shell in wireless example

1,781 Views
chetan98
Contributor II

Hello NXP team,

I am using kw45 loc board to recieve data from multiple sensor through BLE I am using Wireless uart example from sdk I am successfully able to recieve data in ble from multiple device but what i observed shell_dec and shellwrite is taking too much time in printing data in teraterm it is about taking more time in printing data in teraterm.

Almost double the processing time i calculated time using systick freertos tick.

1.I want to know for if nxp can suggest efficient way to printing data multiple byte in less time.

2.And I am using shell present in wireless uart it is blocking or non blocking.

Thankyou 

Chetan

Labels (1)
0 Kudos
Reply
1 Reply

1,734 Views
sofiaurueta
NXP Employee
NXP Employee

Hello,

Hope you are doing well.

 

What SDK version are you using? And what modifications did you implement in the wireless_uart example?

Could you help us explain more details about your application?

 

For wireless UART example, both blocking and non-blocking UART APIs are provided, though it is recommended to use a non-blocking implementation. Blocking functions polls the sending queue, waits for the sending queue to be empty. The non-blocking functions send/receive data using an interrupt method, return directly without waiting for all data written to the transmitter register.

 

The non-blocking implementation uses a ring buffer supported by the transactional receive APIs. Please see the "UART Driver" section from MCUXpresso SDK API Reference Manual for more information.

 

Best Regards,

Ana Sofia.

0 Kudos
Reply