Receiving Device (Coordinator) not updating with End Device Data all the time.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Receiving Device (Coordinator) not updating with End Device Data all the time.

1,154 次查看
matthew3
Contributor III

Hello NXP Community,

I am having trouble receiving from the end device updated data all the time. Sometimes the data gets updated on the receiving device (coordinator) then all of a sudden it stops updating when the end device data changes. I am using the JN-AN-1174 Template as my base template. I using the JN5169 chip i have adapted and added functions to accomadate what i am wanting the two devices to do. I have got communication between the two devices I know this by adding debugs in to help see the process of the program when running.

I just cannot get a stable connection when recieving the data. I have to either reset the end device or the coordinator. Mainly the coordinator more often than the end device.

Please could somebody shed some light on this for me

Regards

Matt

 

0 项奖励
回复
1 回复

1,121 次查看
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi @matthew3,

I hope you are doing great.

I am not sure if I am following your issue, you are working with the Zigbee Home Automation Stack, but I could recommend look at the JN-AN-1229 that follows the same process but with the Zigbee 3.0 Stack.

Is it possible that you could explain your issue again?

Regards,

Mario

0 项奖励
回复