Reading/writing commands on NTAG213

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Reading/writing commands on NTAG213

3,514件の閲覧回数
SabrineG
Contributor I
Hello everyone, I am working on a project to read and write datas on a NTAG213, i am using a customized board which is composed of a DLP RFID2 reader and a CA070 microcontroller. So i am looking for the commands to send to the reader from the CA070 to be able to read and write on the Tag and to secure it. I have already looked on the datasheet but i just can't seem to understand what to used and what to do exactly. so help please!
0 件の賞賛
返信
1 返信

3,498件の閲覧回数
fangfang
NXP TechSupport
NXP TechSupport

Hello,

One may refer to the information as the thread.

URL:https://community.nxp.com/t5/NFC/Ntag-21x-Write-ndef-with-password-protection/td-p/1158260

Hope it help you. Have a nice day.

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

0 件の賞賛
返信