Questions about UWB NCJ29D5 dev kit and UWBMAC-GUI tool

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Questions about UWB NCJ29D5 dev kit and UWBMAC-GUI tool

1,507件の閲覧回数
sjshin
Contributor II

hi,

I connected the MCU+UWB module to a PC via USB and opened the UWBMAC-GUI program.

In the program, I connected the MCU port and clicked the
dialog commands -> UCI core control -> 1.reset the UWBS selected.
But there is no return value from the UWB module.
There is no return value for all commands, not just the "reset the UWBS" command.

The uwb module sw is a pre-flashed sw.

What should I check in this case?
Is there any way to verify that the UWB module is a legitimate module?

ラベル(1)
0 件の賞賛
返信
0 返答(返信)