Hi,
At first, please use two board to do the test of GATT. You should make sense of how this two device works. 'configure gatt server' is used to test the gatt server. In common, we do not use the phone as server. The phone always roles as client. Because server is used to provide the data. and the client shows the data. As to multiple connection, the device don't support by default. You have to realize it by yourself. You can refer the attachment. One for client, one for server.
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------