QN9080 with android

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

QN9080 with android

1,791件の閲覧回数
rakeshmodi
Contributor I

Hello,

I would like to connect  QN9080 based USB dongle with normal android phone using USB C connection. Will this be detected by android device as a serial port or not? If not, how can I use QN9080 based dongle with normal android phone?

 

Thanks,

Rakesh

0 件の賞賛
返信
2 返答(返信)

1,778件の閲覧回数
Ricardo_Zamora
NXP TechSupport
NXP TechSupport

Hello Rakesh,

 

Hope you are doing well. You could use it, but you would need to develop your android application that can interact with the dongle. For the QN9080 side you can use the HCI_BLACK_BOX SDK example. This application implements a Bluetooth Low Energy HCI Black Box.

The android application needs to access the QN9080 using the HCI protocol over serial interface. See the Bluetooth Specification for the format of HCI commands and events over serial interface and the full list of supported commands and events. But at the end, the application development is something you would need to implement by your own.

 

Best Regards,

Ricardo

1,768件の閲覧回数
rakeshmodi
Contributor I

Hello Ricardo,

Thanks for your prompt response. From your response I understand that we will require only user layer android application, and there will be no any changes require to do for Android HAL layer or USB drivers to use QN9080 with android device. Please confirm.

Here I would like to mention that, our intention is not to control/communicate the BLE directly using HCI protocol. We want to detect the NXP device in our Android/iOS as “USB-Serial” device, and handle the message packets sent over the USB-Serial via our proprietary protocol on android/iOS. 

Thanks,

Rakesh

0 件の賞賛
返信