QN9080 reflow profile

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

QN9080 reflow profile

Jump to solution
2,449 Views
benjaminchang
Contributor V

Hi,

We are designing QN9080 board.

We need QN9080 reflow profile data, but cannot find it from datasheet or AN11996_QN908x Hardware Design Considerations_v13.

We searched and found related data from section 12.3 Reflow profile of QN9080-001-M17.pdf (SIP).

Can we use this SIP data for QN9080 IC, or there are other profile data? Please provide.

y1.png

Regards,

Benjamin

Labels (1)
  • QN

0 Kudos
Reply
1 Solution
2,339 Views
benjaminchang
Contributor V

Hi Andrea,

Thanks for your fast response. Thank you!

Regards,

Benjamin

View solution in original post

0 Kudos
Reply
3 Replies
2,339 Views
nxf54943
NXP Employee
NXP Employee

Dear Benjamin Chang,

If you check the part Quality Information you can see it can support 240C° if the solder has lead or 260C°  if it is lead free, this can be check on the following link: https://www.nxp.com/part/QN9080DHN

You can also follow the Recommended Reflow Soldering Profile which can be use for this part https://www.nxp.com/docs/en/supporting-information/Reflow_Soldering_Profile.pdf

Kind regards, Andrea.

0 Kudos
Reply
2,329 Views
tigerzhu
Contributor I

We need LPC1768 reflow profile data.

0 Kudos
Reply
2,340 Views
benjaminchang
Contributor V

Hi Andrea,

Thanks for your fast response. Thank you!

Regards,

Benjamin

0 Kudos
Reply