QN9020 fail to download

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

QN9020 fail to download

ソリューションへジャンプ
3,807件の閲覧回数
Doomer
Contributor II

Hi

I managed to download the bin file under \BinFiles\BinFiles_B2_v40 from ISP

But after I download the keil built bin file from ISP or directly download from keil(using code under \Projects\BLE), the board isn't working properly, leds off and no response pushing the buttons.

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
3,745件の閲覧回数
estephania_mart
NXP TechSupport
NXP TechSupport

Hello,

 

Could you please help me confirm you are using Bluetooth LE version 4.2? You will need to be sure to be using the qn9020b4_lib_peripheral_v42.a library

 

Regards,

 

元の投稿で解決策を見る

0 件の賞賛
返信
7 返答(返信)
3,790件の閲覧回数
estephania_mart
NXP TechSupport
NXP TechSupport
0 件の賞賛
返信
3,774件の閲覧回数
Doomer
Contributor II

I think I have correctly set the options in keil, but the board still failed to work properly.

0 件の賞賛
返信
3,761件の閲覧回数
estephania_mart
NXP TechSupport
NXP TechSupport

Hello,

 

Could you please provide more details on which example are you using ? Are you using the low power capabilities ?

 

Regards,
Estephania

0 件の賞賛
返信
3,758件の閲覧回数
Doomer
Contributor II

The broadcaster example. I didn't change the code.

0 件の賞賛
返信
3,746件の閲覧回数
estephania_mart
NXP TechSupport
NXP TechSupport

Hello,

 

Could you please help me confirm you are using Bluetooth LE version 4.2? You will need to be sure to be using the qn9020b4_lib_peripheral_v42.a library

 

Regards,

 

0 件の賞賛
返信
3,714件の閲覧回数
Doomer
Contributor II

I repaired the SDK and finally solved the problem.

Thanks a lot.

0 件の賞賛
返信
3,738件の閲覧回数
Doomer
Contributor II

Under QN902x_SDK_1.4.0\Projects\BLE\src\lib, I can only find qn9020b0_lib_peripheral,qn9020b1_lib_peripheral and qn9020b2_lib_peripheral for keil and IAR.

0 件の賞賛
返信