QN9020 fail to download

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

QN9020 fail to download

跳至解决方案
3,701 次查看
Doomer
Contributor II

Hi

I managed to download the bin file under \BinFiles\BinFiles_B2_v40 from ISP

But after I download the keil built bin file from ISP or directly download from keil(using code under \Projects\BLE), the board isn't working properly, leds off and no response pushing the buttons.

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
3,639 次查看
estephania_mart
NXP TechSupport
NXP TechSupport

Hello,

 

Could you please help me confirm you are using Bluetooth LE version 4.2? You will need to be sure to be using the qn9020b4_lib_peripheral_v42.a library

 

Regards,

 

在原帖中查看解决方案

0 项奖励
回复
7 回复数
3,684 次查看
estephania_mart
NXP TechSupport
NXP TechSupport
0 项奖励
回复
3,668 次查看
Doomer
Contributor II

I think I have correctly set the options in keil, but the board still failed to work properly.

0 项奖励
回复
3,655 次查看
estephania_mart
NXP TechSupport
NXP TechSupport

Hello,

 

Could you please provide more details on which example are you using ? Are you using the low power capabilities ?

 

Regards,
Estephania

0 项奖励
回复
3,652 次查看
Doomer
Contributor II

The broadcaster example. I didn't change the code.

0 项奖励
回复
3,640 次查看
estephania_mart
NXP TechSupport
NXP TechSupport

Hello,

 

Could you please help me confirm you are using Bluetooth LE version 4.2? You will need to be sure to be using the qn9020b4_lib_peripheral_v42.a library

 

Regards,

 

0 项奖励
回复
3,608 次查看
Doomer
Contributor II

I repaired the SDK and finally solved the problem.

Thanks a lot.

0 项奖励
回复
3,632 次查看
Doomer
Contributor II

Under QN902x_SDK_1.4.0\Projects\BLE\src\lib, I can only find qn9020b0_lib_peripheral,qn9020b1_lib_peripheral and qn9020b2_lib_peripheral for keil and IAR.

0 项奖励
回复