QN9020 Over The Air (OTA) firmware update support

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

QN9020 Over The Air (OTA) firmware update support

3,345 次查看
hugh_okeeffe
Contributor I

Question 1:

 

We tried to get the sample OTA server (that comes in the SDK) to execute on the QN9020_MINIDK_V8 eval board, for evaluation purposes. During initialization, the sample OTA server is calling a library function (otas_init) where the expected return code is OTA_STATUS_OK. However the function is instead returning OTA_STATUS_DEVICE_NOT_SUPPORT_OTA. i.e. The OTAS initialization failed; the device does not support OTA.

Would like to know under what conditions this error gets returned?

 

Question 2:

 

The document says:

 

OTA clients for Android and IOS can be downloaded from Collabnet which is an NXP customer support site.  

Could we get direct download links for these OTA clients for testing purposes? I haven't had success in finding them online.

 

Thanks

Hugh

标签 (2)
标记 (2)
0 项奖励
回复
5 回复数

3,077 次查看
Corgi
Contributor II

Could I get direct download links for these OTA clients for testing purposes? I haven't had success in finding them online, too

0 项奖励
回复

3,071 次查看
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi @Corgi,

You could download the SDK following the next page QN9020.

Regards,

Mario

0 项奖励
回复

3,060 次查看
Corgi
Contributor II

OTA clients for Android and IOS can be downloaded from Collabnet which is an NXP customer support site.  

Is it means that SDK Example , Not iOS or Android Example

 

--

Regards

Corgi

0 项奖励
回复

3,036 次查看
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi @Corgi,

We going to handle this matter internally.

Mario

0 项奖励
回复

3,228 次查看
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Hugh,

Question 1:

 

Would like to know under what conditions this error gets returned?

You need to flash the bin file using the ISP Studio, selecting the OTA  option.

pastedImage_1.png

Question 2.

I get back to you internally.

Regards,

Mario

0 项奖励
回复