PN533 - Emulate type 4 tag A with libnfc

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PN533 - Emulate type 4 tag A with libnfc

1,223 Views
Horia_Ciulica
Contributor I

Hello,

So i'm trying to emulate a type 4 tag-A using a PN533 dongle and libnfc. I've tried with example from nfc-tools "nfc-forum-tag4" and with "nfc-emulate-uid" (adding nfc_target_receive_bytes instead of nfc_target_receive_bits), the problem is that nfc_target_receive_bytes crash my application. The question is: can i do this using PN533 or i need to use another device, and if the answer is yes what device works fine with this type of emulation?

0 Kudos
Reply
2 Replies

1,169 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi Horia:

PN533 is not recommended for new designs. Please refer to below link for more details.

https://www.nxp.com/products/rfid-nfc/nfc-hf/nfc-readers/usb-nfc-integrated-solution:PN5331B3HN

 

It is possible for PN533 to emulate type 4,  for your question, it will need more information for further analyzing, include the project source files.

 

Regards

Daniel

0 Kudos
Reply

1,131 Views
Horia_Ciulica
Contributor I

Hello Daniel,

Thank you for reply, I'm new on this part what do you mean "new design", and PN7462 do you think it's the best solution for using with Nfc-forum-4tag?

0 Kudos
Reply