PDM: Unexpected call back Code 3 Number 61698

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PDM: Unexpected call back Code 3 Number 61698

1,111 Views
xubovey
Contributor III

hi,

thanks

i get the err log in the function, and most time it work well,

the log was:

err:

[07:41:38.180] PDM: Unexpected call back Code 3 Number 61698

[07:41:38.272] PDM: Unexpected call back Code 3 Number 61700

[07:41:38.272] PDM: Unexpected call back Code 3 Number 61697

[07:41:38.293] PDM: Unexpected call back Code 3 Number 61699

[07:41:38.311] PDM: Unexpected call back Code 3 Number 61697

[07:41:38.320] PDM: Unexpected call back Code 3 Number 61699

right:

[07:41:34.183] NodeNum: 0, NwkAddr: 0x9cc8, IeeeAddr:00158d000211ff3b.

[07:41:34.190] NodeNum: 1, NwkAddr: 0xfffe, IeeeAddr:0000000000000000.

the code was:

PUBLIC uint8 app_u8MacAddrAndIeeeAddrPrint(void)
{
uint16 u16DstAddr;
uint16 nodeNum = 0;

do
{
u16DstAddr = ZPS_u16AplZdoLookupAddr(ZPS_u64NwkNibGetMappedIeeeAddr(ZPS_pvAplZdoGetNwkHandle(),nodeNum));
DBG_vPrintf(TRACE_APP, "NodeNum: %d, NwkAddr: 0x%04x, IeeeAddr:%016llx.\n",
nodeNum,
u16DstAddr,
ZPS_u64NwkNibGetMappedIeeeAddr(ZPS_pvAplZdoGetNwkHandle(),nodeNum));
nodeNum ++;
}while (0xFFFE != u16DstAddr);

return nodeNum;
}

what should i do to fix the bug, thanks for your help!

Labels (3)
Tags (2)
0 Kudos
Reply
1 Reply

1,033 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Xu,

I am not sure what is the values that you want.

Did you look at the appZpsExtendedDebug.c file?

C:\NXP\bstudio_nxp\sdk\JN-SW-4170\Components\ZigbeeCommon\Source\appZpsExtendedDebug.c

Regards,

Mario

0 Kudos
Reply