OM2NTP5332 board Output voltage only 0.176V,How to set the voltage output to 2.5V

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

OM2NTP5332 board Output voltage only 0.176V,How to set the voltage output to 2.5V

850 Views
liyidreamer
Contributor I

Hello,

 

I am evaluating energy harvesting function on OM2NTP5332 board,I am testing the OM2NTP5332 board with App "NTAG5 - Dev. kit Use Cases", after sending some commands to the board,Output voltage only 0.176V.using App "Xplore NTAG 5",Output voltage only 0.176V.

Is there any way to restore the circuit board so that the Vout voltage output can be configured to 2.5V? thanks!

0 Kudos
Reply
1 Reply

815 Views
fangfang
NXP TechSupport
NXP TechSupport

Hello @liyidreamer .

Please kindly refer to the 4.2.8 EH & ED settings of the UM11207 as the link.

URL:https://www.nxp.com.cn/docs/en/user-guide/UM11207.pdf.

Have a nice day.

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

 

0 Kudos
Reply