Hello NXP team,
I'm trying to program the PNEV7462C with some example project from the PN7462AU FW and SW Examples Full Version - v06.10.00 zip file (SW3683.zip). When I try to guild a project MCUxpresso give me the following error:
----
**** Build of configuration DebugPN7462AU for project PN7462AU_ex_phExVCom_mcux ****
Nothing to build for project PN7462AU_ex_phExVCom_mcux
----
I downloaded and uploaded the SDK from the FRDM-K82F board in the 'Installed SDKs' window (SW3827.zip : SDK_2.x_FRDM-K82F). I imported the example with the 'Import project(s) from file system...' function from the Quickstart menu and pointed it to the SW3683.zip file. When I imported it only the mucx extension (<project name>_mcux) project appeared and when I tried to build it the discussed error popped-up.
Can you help me find out what have I done wrong ?
Best regards,
Alexandre Pellerin.