Network key disabled

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Network key disabled

跳至解决方案
2,158 次查看
jasonchiang
NXP Employee
NXP Employee

Hi,

  Under Beekit configuration, there is network key setup. If the value is set all 00s, the trust center will generate a random network key.

How to disable this network key setup ? As I would like to see ASDU data without any security. What kind of security key used in current default images under Zed1.6.5/Embedded/KW24D512TwrHa/


0 项奖励
回复
1 解答
1,960 次查看
AngelC
Senior Contributor I

Dear Tzyy-Hong,

If you would like to modify the security settings of the images used in ZeD 1.6.5 you should first open the corresponding BeeKit solution file located in folder: C:\Program Files (x86)\Freescale\ZeD 1.6.5\BeeKitSolutionFiles.

In this case it would be the ZigBeeHcApps_TWR_KW24D512_CB401.bksln or, ZigBeeHcApps_TWR_KW24D512_CB400.bksln depending in the codebase you have in BeeKit. Once open, you may see all of the projects in the right side under “Project explorer”, see image below:

Capture5.PNG.png

There you may click on “BeeStack” and change the stack profile to “No security with mesh routing – Stack Profile 2”.

IMPORTANT: Use this only for testing purposes. Real ZHA application may require security settings.

Regards,

AngelC

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,961 次查看
AngelC
Senior Contributor I

Dear Tzyy-Hong,

If you would like to modify the security settings of the images used in ZeD 1.6.5 you should first open the corresponding BeeKit solution file located in folder: C:\Program Files (x86)\Freescale\ZeD 1.6.5\BeeKitSolutionFiles.

In this case it would be the ZigBeeHcApps_TWR_KW24D512_CB401.bksln or, ZigBeeHcApps_TWR_KW24D512_CB400.bksln depending in the codebase you have in BeeKit. Once open, you may see all of the projects in the right side under “Project explorer”, see image below:

Capture5.PNG.png

There you may click on “BeeStack” and change the stack profile to “No security with mesh routing – Stack Profile 2”.

IMPORTANT: Use this only for testing purposes. Real ZHA application may require security settings.

Regards,

AngelC

0 项奖励
回复