NFC mode

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决
6,952 次查看
Alanking
Contributor II

Hi,

    we want to use NFC as our BLE pairing out band interface,so we expect that the NFC chip can worked at the Card emulation and Reader/writer mode at the same time,Does NFC support this application scenario?And are there any recommended chips or mature solutions?

    Thank you so much.

    

0 项奖励
回复
1 解答
6,856 次查看
fangfang
NXP TechSupport
NXP TechSupport

Hello,

Thanks for your information. Actually we don't recommend PN532 for new design(So there is no information on NXP website), we recommend PN7120 or PN7150 instead, and there is source code as the below:

NXP-NCI MCUXpresso example Project  

 

 

Have a nice day.

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
5 回复数
6,938 次查看
fangfang
NXP TechSupport
NXP TechSupport

Hello,

>> we expect that the NFC chip can worked at the Card emulation and Reader/writer mode at the same time.
NXP reader can support Card emulation or Reader/writer mode. But can not be at the same time.
For the more information please refer to the link.
URL: https://www.nxp.com/products/rfid-nfc/nfc-hf/nfc-readers:NFC-READER

 

Have a nice day.

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

0 项奖励
回复
6,919 次查看
Alanking
Contributor II

Thank you for your reply.

I want to know whether this simultaneous working mode is not supported by the NXP chip, the NFC protocol, or neither?

In mobile phone applications, the mobile phone can act as a card or a card reader. Does this mean that two NFC chips are integrated in the phone, or that there is only one NFC chip but the two modes work in time sharing?

In our application, we hope that both parties in communication can actively obtain each other's information. Because we want to support LE Legacy Pairing and LE Secure Connections Pairing at the same time, LE Legacy Pairing requires both parties to obtain each other's OOB data before they can pair. So is only the P2P mode of NFC available? Or you have a better opinion.

thanks. 

 

标记 (1)
0 项奖励
回复
6,891 次查看
fangfang
NXP TechSupport
NXP TechSupport

Hello,

Thanks for your update information.

For your detail information you may contact our partner as the link.

URL:https://www.nxp.com/products/rfid-nfc/rfid-ecosystem:RFID_ECOSYSTEMS.

Have a nice day.

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

0 项奖励
回复
6,873 次查看
Alanking
Contributor II

ok, I know, thank you.

We plan to use PN532, where can I download the official PN532 library for full mode? I looked for it on the NXP official website, but I couldn't find the corresponding one.

标记 (1)
0 项奖励
回复
6,857 次查看
fangfang
NXP TechSupport
NXP TechSupport

Hello,

Thanks for your information. Actually we don't recommend PN532 for new design(So there is no information on NXP website), we recommend PN7120 or PN7150 instead, and there is source code as the below:

NXP-NCI MCUXpresso example Project  

 

 

Have a nice day.

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

0 项奖励
回复