NFC Cockpit connect error with CLEV6630B

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NFC Cockpit connect error with CLEV6630B

Jump to solution
2,594 Views
jenny_nfc
Contributor I

hi,

  It's the 1st time I use CLEV6630B(RC663).

  The Cockpit v6.50 and VCOM.bat have been installed.

   But when Cockpit opened,Log Monitor says:

ERROR:ServiceFactory:Bal, Hal, OSal Initialization (VCOM_RC663 @COM3) Failed with GENERIC,USE_CONDITION

  How can I solve the problem?Thanks.

CockpitError.PNG

Tags (1)
0 Kudos
Reply
1 Solution
2,554 Views
fangfang
NXP TechSupport
NXP TechSupport

Hello @jenny_nfc .

Thanks for your information.
In order to better service for you, would you please kindly provide the below information?
Firstly. Did you follow the step of 3. Software as the AN11022 as the link?
URL:https://www.nxp.com.cn/docs/en/application-note/AN11022.pdf.
Secondly. Did you test Cockpit V6.3 and  has the same question?

 

Have a nice day.

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
1,485 Views
imx8-mdt
Contributor I

Hi  

have you addressed this connection issue?

I have the same issue to connect CLEV6630B with Cockpit v8.0.

I think the vcom driver has been installed ,as I can see the COM30 show up in my windows10 device manager.

I just tear down the package of CLEV6630B today. so I think the default firmware in it should work for Cockpit reading/writing.

 

Could anyone help on this? Thanks

imx8mdt_0-1716545482794.png

 

Tags (1)
0 Kudos
Reply
2,555 Views
fangfang
NXP TechSupport
NXP TechSupport

Hello @jenny_nfc .

Thanks for your information.
In order to better service for you, would you please kindly provide the below information?
Firstly. Did you follow the step of 3. Software as the AN11022 as the link?
URL:https://www.nxp.com.cn/docs/en/application-note/AN11022.pdf.
Secondly. Did you test Cockpit V6.3 and  has the same question?

 

Have a nice day.

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

0 Kudos
Reply