Manufacture specific commands using NXP ZigBee HA demo application

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Manufacture specific commands using NXP ZigBee HA demo application

1,863件の閲覧回数
nisarg_parmar
Contributor I

Can someone suggest a reference material for JN5169 to achieve functionality mentioned below?

  1. Manufacturer specific custom command in On/OFF cluster for HA profile.
    We want send manufacturer specific data (for control & pattern on 4x4 RGB click) from JN5169 coordinator(UART connection between Gateway linux and JN5169 coordinator) to JN5169 Zigbee ED.
  2. Send above command from JN5169 coordinator as Multicast in Zigbee network.

Using following SDK as a starting point.

  • JN-SW-4168 - JN516x ZigBee Home Automation SDK
  • JN-AN-1189 - ZigBee Home Automation Demonstration Application Note
0 件の賞賛
返信
1 返信

1,560件の閲覧回数
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Nisarg,

You can take a look the next application notes.

ZigBee Home Automation|NXP  The app note JN-AN-1223

Also the JN-AN-1184 could help you with the Zigbee Coordinator.

The App note provides the documentation for each example.

Hope it helps.

Best Regards,

Mario

0 件の賞賛
返信