Manual update SDK library, the device can't connect after pairing

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Manual update SDK library, the device can't connect after pairing

Jump to solution
2,692 Views
wang_barry
Contributor III

Hello,

My design board used QN9083.

The project first has created from SDK_2.x_QN908CD 2.2.1 bluetooth_heart_rate_sensor_freertos example. 

In order to update SDK to SDK_2.x_QN908CD 2.2.2,  I replace framework / bluetooth/ libs manually (include lib_ble_5-0_host_peripheral_cm4.a / lib_ble_QN908XC_controller.a / lib_crypto_m4.a) and also enabled pairing and bonding (gAppUseBonding_d  & gAppUsePairing_d). 

After updating SDK, the device can't re-connect after pairing successful.

PS: without updating SDK. the reconnect is successful after pairing successful but enable gAppUseNvm_d not work.

Any step should I do before update SDK?

 

0 Kudos
Reply
1 Solution
2,639 Views
wang_barry
Contributor III

Hello @estephania_mart 

 

 Yes, it seems to have the latest SDK version 2.2.5 that released in 2021.03.10

   I should update it

wang_barry_0-1615786677397.png

 Regards,

 Barry Wang

View solution in original post

4 Replies
2,674 Views
estephania_mart
NXP TechSupport
NXP TechSupport

Hello,

 

In this case for this type of migration we recommend it to do it the other way around. As there are always improvements in the libraries, there might be also some minor changes or some variables naming conventions that could be affected that the library might be looking for but the current code will not have , so in this case the migration should be made the other way around, it will be needed for you to move your application to the new SDK SW using some example as a base.

 

Also, please help me verify for the latest version of the SDK in the MCUXpresso Dashboard.

 

Regards,

Estephania

 

0 Kudos
Reply
2,660 Views
wang_barry
Contributor III

Hello @estephania_mart 

Got it, below is the SDK version screenshot from MCUXress IDE

01.png

0 Kudos
Reply
2,656 Views
estephania_mart
NXP TechSupport
NXP TechSupport

Hello,

 

Could you please help me check the MCUXpresso Dashboard? I believe that there was a new version released on Monday

 

Regards,
Estephania

0 Kudos
Reply
2,640 Views
wang_barry
Contributor III

Hello @estephania_mart 

 

 Yes, it seems to have the latest SDK version 2.2.5 that released in 2021.03.10

   I should update it

wang_barry_0-1615786677397.png

 Regards,

 Barry Wang