MMZ09332BT1: Difference between data sheet and s-parameters in s2p file

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MMZ09332BT1: Difference between data sheet and s-parameters in s2p file

1,637件の閲覧回数
elliottaylor
Contributor I

Hi,

I am interested in using the MMZ09332BT1 in one of my projects which will incorporate the amplifier into an RF transmitter, transmitting at 145MHz. I was comparing the input return loss on the data sheet to that given in the s-parameters file for my frequency. In the data sheet (http://cache.freescale.com/files/rf_if/doc/data_sheet/MMZ09332B.pdf) the graph shows an input return loss of around -15 to -20 (pg.21). The s2p file however, shows an s11 magnitude of 0.626794634 for 144MHz. In dB this is 20log(0.627) which is only ~ -4dB.

Why is there this large difference and which value should I take to be more accurate?

Also is there a 1db compression point value and a ACPR value available for the frequency range of 136–174 MHz?

Thanks in advance for any help.

Cheers

Elliot

ラベル(1)
0 件の賞賛
返信
0 返答(返信)