Hi,
How we can write and read MAC address for KW40/41 MCUs. If we need to use the blhost, please let me know, how to use that.. (Read Once Command, Program Once Command ).
Thanks
已解决! 转到解答。
The way you program different MAC addresses in production is by using a programmer with serialization capabilities (i.e. P&E Cyclone Max). In our stack, the MAC Address is stored in a global variable under the name gBDAddress_c. First you need to open the .map file that is generated in you code, look for this variable and get where it is located in flash.
Once you have the variable address, you can now use the same binary to program all the MCUs and use the serialization tool to overwrite only the memory location that contains the MAC address. Instructions for doing this will depend on the flashing tool you will use in production. Attached you will find some instructions on how to do it using the Cyclone Max.
Hope it helps.
Best Regards
Thanks for all the clarifications. For completeness, if you could provide us the instruction for writing to that specific address using "blhost" or any other tool, it would be useful.
Hi Chiang,
Thanks a lot for this information, it is really useful.
Hi sensenthuran
Kinetis bootloader hasn?t been ported to be used with the connectivity software. Connectivity software uses a custom linker file that is not compatible with Kinetis bootloader and hence it is not included in the connectivity software stack. The only way to change the MAC address right now is trought the manufacturing tools with serialization capabilities available in the market.
Best Regards
KW41 has kinetis bootloader:
# ./blhost -p /dev/ttyMSM1 -- get-property 1
Ping responded in 1 attempt(s)
Inject command 'get-property'
Response status = 0 (0x0) Success.
Response word 1 = 1258422272 (0x4b020000)
Current Version = K2.0.0
Hi sensenthuran
How are you connecting with the KW41 (USB port J6 in FRDM, UART Pins PTC7 and PTC7)? Also, are you flashing any example firmware from the Connectivity Software Package?
Saludos
Hi sensenthuran!
Many production programmers for Kinetis have serialization capability to program MAC addresses. P&E Micro has the Cyclone Max, Cyclone Universal, and Cyclone Universal FX. In addition to the serialization tool that was mentioned by the other poster, we also have tools that allow you to program it through a DLL or scriptable application.
Please visit us at our website if you have any questions.
Regards,
Johnny
P&E Microcomputer Systems, Inc.
Hi @Jose Santiago Lopez Ramirez
I found the memory location of variable "gBDAddress_c" is different in each App.
For example, that is the point what I found as below.
In heart_rate_sensor_BM.map:
gBDAddress_c 0x000225e8
In hci_app_BM.map:
gBDAddress_c 0x00014094
Does it mean that we need to overwrite the memory location again after we update another Apps on our unit?
For example, if we have heart_rate_sensor_app on KW41Z first then we program different MAC addresses on each unit.
After that we update hci_app on it, do we need to program MAC address again?
Is there any way to write MAC address into KW41Z that it may not be affected by different Apps?
Thanks
Hi Leo,
For KDS and more generally for GCC please refer to the below post:
https://mcuoneclipse.com/2012/11/01/defining-variables-at-absolute-addresses-with-gcc/
Cheers,
Antonio
Hi Leo,
You are right, the memory location of the MAC address holding arraywill change with every application or even in the same application if the application code changes. To overcome this you need to make sure that this variable will have always the same location in memory. This has a different procedure depending on the IDE you are using. In IAR for example, adding a pragma before the variable in question does the trick.
#pragma location=address
char variable[size];
Saludos
Santiago López
Thanks a lot @Jose Santiago Lopez Ramirez for the quick reply with detailed answer. Appreciate your help.
The way you program different MAC addresses in production is by using a programmer with serialization capabilities (i.e. P&E Cyclone Max). In our stack, the MAC Address is stored in a global variable under the name gBDAddress_c. First you need to open the .map file that is generated in you code, look for this variable and get where it is located in flash.
Once you have the variable address, you can now use the same binary to program all the MCUs and use the serialization tool to overwrite only the memory location that contains the MAC address. Instructions for doing this will depend on the flashing tool you will use in production. Attached you will find some instructions on how to do it using the Cyclone Max.
Hope it helps.
Best Regards
Thanks @Jose Santiago Lopez Ramirez for your detail answer. How we can program different MAC address for different KW40/41. Do we need to compile every time or can we load the same binary and use any utilities/tools to write different MAC address in the factory?
Hi sensenthuran,
On the BLE Host Stack, the device MAC addresses are defined at compile time. For each device, the MAC address can be modified in the app_preinclude.h file.
If you want to read a MAC address from the BLE Client you must call the function Gap_ReadPublicDeviceAddress (in our demos it is called in the function BleApp_Config in app.c). After this, the gPublicAddressRead_c event will occur every time a new MAC address is discovered. You must obtain these MAC addresses in the BleApp_GenericCallback (in app.c) by reading the pGenericEvent pointer as shown in the image below.
Every time a new MAC address is found nearby, this callback function will be called.
Let me know if this is what you are looking for.
Best Regards