Kinetis BLE Toolbox - Wireless UART will not pair

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Kinetis BLE Toolbox - Wireless UART will not pair

5,342 次查看
toddcomins
Contributor II

I cannot get the Android Kinetis BLE Toolbox to pair with the FRDM-KW41Z board running the Hybrid Thread/BLE UART or BLE UART project. I can see the board show up as NXP_THR in the available devices list under Android BlueTooth settings... but never in the BLE Toolbox app. Any suggestions?

标签 (3)
9 回复数

4,319 次查看
toddcomins
Contributor II

Turning on GPS was the fix! Thanks for the help.

4,319 次查看
sterenn
Contributor II

Hello, 

How did you manage to pair your phone with the board ? For me, the phone is able to connect to the board, but no interaction is possible as long as the phone (or PC) asks for a pairing code (and both 0000 and 1234 won't work). 

Thank you,

0 项奖励
回复

4,319 次查看
toddcomins
Contributor II

We do not pair the board with the phone before launching the IoT Toolbox app (on Android). 

We turn on Bluetooth, turn off GPS, and then launch the NXP IoT Toolbox app. On the IoT Toolbox app screen we select the Wireless Console/UART icon. On the next screen the board we select the board and then we get the console screen. Sometimes, we have to exit the IoT Toolbox app and turn off Bluetooth, turn on Bluetooth, and then launch the IoT Toolbox app again. But for the most part, it works fine.

4,319 次查看
Lupo
Contributor III

I would hardly think that by myself, testing the uart!

Thanks a lot

0 项奖励
回复

4,319 次查看
toddcomins
Contributor II

I can try an older phone tomorrow. I'm not familiar with security settings on Android related to BlueTooth so I'll have to investigate that.

FYI - I'm using Kinetis LBE Toolbox release data 02-21-2017 Version 5.0.0.

0 项奖励
回复

4,319 次查看
albertovargas
NXP Employee
NXP Employee

You can also try

  • disable wi-fi on your smartphone
  • make sure that location services are enabled (Since Android 6.0, location services need to be enabled in order to locate BLE devices)
  • make sure the location services permission was granted to the app

On the embedded side, are you using both Hybrid Thread/BLE UART with default settings?

4,319 次查看
toddcomins
Contributor II

Google Pixel phone, Android Version 7.1.1.

0 项奖励
回复

4,319 次查看
albertovargas
NXP Employee
NXP Employee

I did a quick test, I was able to perform a connection using a Nexus 6 with Android 7.0 and a Nexus 5X running 7.1.1 using Wireless UART firmware with default settings. By chance, do you have any older phone to use for testing? Also, are you using security parameters by default?

0 项奖励
回复

4,319 次查看
albertovargas
NXP Employee
NXP Employee

Hi Todd,

Could you please provide your smartphone brand, model and Android version?

0 项奖励
回复