KW45 - How to programe a new board without debug ic ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

KW45 - How to programe a new board without debug ic ?

跳至解决方案
2,141 次查看
james1z1j
Contributor I

hi :

       Can you help me ? I had a KW45 board without debug ic(It like kw45 evm board,but no LPC55S69JBD100) .I want to programe it .but i have to burn the image of NBU(SB3 file).I have opened urat1 in isp model.but when I burned the SB3 file ,it display timeout error.If I need to load bootload to the board before burning the SB3 file .

 

have good day!

james

0 项奖励
回复
1 解答
2,107 次查看
Ricardo_Zamora
NXP TechSupport
NXP TechSupport

Hello,

 

Hope you are doing well. Could you please help me checking these Application Notes?

 

Hope this helps.

 

Best Regards,

Ricardo

在原帖中查看解决方案

3 回复数
1,980 次查看
justinleeyang
Contributor III

The above document does not explain how to download the program to kw45. Is it possible to directly provide the code and bin file that can be burned for download and testing By only SWD ?

0 项奖励
回复
2,108 次查看
Ricardo_Zamora
NXP TechSupport
NXP TechSupport

Hello,

 

Hope you are doing well. Could you please help me checking these Application Notes?

 

Hope this helps.

 

Best Regards,

Ricardo

2,077 次查看
james1z1j
Contributor I
Thanks ,th fuses must be right.
0 项奖励
回复