KW45 - How to programe a new board without debug ic ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KW45 - How to programe a new board without debug ic ?

ソリューションへジャンプ
2,060件の閲覧回数
james1z1j
Contributor I

hi :

       Can you help me ? I had a KW45 board without debug ic(It like kw45 evm board,but no LPC55S69JBD100) .I want to programe it .but i have to burn the image of NBU(SB3 file).I have opened urat1 in isp model.but when I burned the SB3 file ,it display timeout error.If I need to load bootload to the board before burning the SB3 file .

 

have good day!

james

0 件の賞賛
返信
1 解決策
2,026件の閲覧回数
Ricardo_Zamora
NXP TechSupport
NXP TechSupport

Hello,

 

Hope you are doing well. Could you please help me checking these Application Notes?

 

Hope this helps.

 

Best Regards,

Ricardo

元の投稿で解決策を見る

3 返答(返信)
1,899件の閲覧回数
justinleeyang
Contributor III

The above document does not explain how to download the program to kw45. Is it possible to directly provide the code and bin file that can be burned for download and testing By only SWD ?

0 件の賞賛
返信
2,027件の閲覧回数
Ricardo_Zamora
NXP TechSupport
NXP TechSupport

Hello,

 

Hope you are doing well. Could you please help me checking these Application Notes?

 

Hope this helps.

 

Best Regards,

Ricardo

1,996件の閲覧回数
james1z1j
Contributor I
Thanks ,th fuses must be right.
0 件の賞賛
返信