KW45 - How to programe a new board without debug ic ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KW45 - How to programe a new board without debug ic ?

Jump to solution
2,131 Views
james1z1j
Contributor I

hi :

       Can you help me ? I had a KW45 board without debug ic(It like kw45 evm board,but no LPC55S69JBD100) .I want to programe it .but i have to burn the image of NBU(SB3 file).I have opened urat1 in isp model.but when I burned the SB3 file ,it display timeout error.If I need to load bootload to the board before burning the SB3 file .

 

have good day!

james

0 Kudos
Reply
1 Solution
2,097 Views
Ricardo_Zamora
NXP TechSupport
NXP TechSupport

Hello,

 

Hope you are doing well. Could you please help me checking these Application Notes?

 

Hope this helps.

 

Best Regards,

Ricardo

View solution in original post

3 Replies
1,970 Views
justinleeyang
Contributor III

The above document does not explain how to download the program to kw45. Is it possible to directly provide the code and bin file that can be burned for download and testing By only SWD ?

0 Kudos
Reply
2,098 Views
Ricardo_Zamora
NXP TechSupport
NXP TechSupport

Hello,

 

Hope you are doing well. Could you please help me checking these Application Notes?

 

Hope this helps.

 

Best Regards,

Ricardo

2,067 Views
james1z1j
Contributor I
Thanks ,th fuses must be right.
0 Kudos
Reply