KW38 32MHz oscilator could not work

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KW38 32MHz oscilator could not work

1,370件の閲覧回数
Wade1
Contributor I

Hi, dear Sir/Madam

     I have used KW38 on my board. The 32MHz oscilator didn't work after booting. After switching to FEE mode by setting MCG_C1->CLKS as 00 and MCG_C1->IREFS as 0,the MCG_S->IREFST will keep high and not be set as 0 as expected,thus the mode Switching fails and stuck in the while loop.

The schemetic of KW38 is the following picture. The components which have the "*" value are DNP components.

Wade1_0-1629805385369.png

I am sure the oscilator is well, because I have put it on the Freedom board. Ant it  worked well. It's like something wrong with my hardware. But I can't find it. Could you help me fix it.

Thanks!

タグ(1)
0 件の賞賛
返信
1 返信

1,334件の閲覧回数
Ricardo_Zamora
NXP TechSupport
NXP TechSupport

Hi,

 

Hope you are doing well. Are you connecting your 32M XTAL to pins 29 (XTAL_OUT) and 31 (XTAL)?

Could you please check the Hardware Design Files of our FRDM-KW38?

There you can see that our 32MHz XTAL is connected to pins 30 (EXTAL) and 31 (XTAL).

 

Best Regards,

Ricardo