KW36, using 32MHZ XO in FEE mode and the power consumption is too high

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KW36, using 32MHZ XO in FEE mode and the power consumption is too high

2,526件の閲覧回数
jictannu
Contributor III

According to the KW35_36_BLE_power_profile_calculator_v0p9, the adverting interval is 100ms, the processor configuration is 32MHZ FEE using 32MHz XO, the average radio current is 0.4mA. my configuration is fee using 32MHZ XO, bus clock is 20MHZ, the average radio current is about 3mA. Am I configured wrong somewhere? But when my configuration is 20.97MHz FEI using 32kHz IRC, the average radio current is similar to the calculator.

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

2,495件の閲覧回数
Sebastian_Del_Rio
NXP Employee
NXP Employee

I hope you're doing well!

 

Could you please confirm on which SDK example did you perform your modifications?

 

Could you please confirm if you have you disabled all of the unused modules in your project?

 

Best regards,

Sebastián

0 件の賞賛
返信

2,485件の閲覧回数
jictannu
Contributor III

Hi, Sebastián. I use SDK 2.2.5, HRS demo. I only change the clock configuration.

0 件の賞賛
返信

2,462件の閲覧回数
Sebastian_Del_Rio
NXP Employee
NXP Employee

Hi @jictannu,

 

The power profiling calculator tool is designed to provide an approximation to the amount of power that a certain configuration in the KW36 that can be expected.

 

However, the results provided by this tool are not definitive, and variations may occur for different reasons, as even the physical design of the PCB, some of the peripherals, or even an additional LED being on can change the results of the power measurement. The measurement method itself can also cause variations in the power readings.

 

Please let me know if you need any more information.

 

Best regards,

Sebastián

0 件の賞賛
返信