KW35, KW38, KW45, KW47 & MCX W71, MCX W72 & MCX W23 Power Profile Tools (including Localization)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KW35, KW38, KW45, KW47 & MCX W71, MCX W72 & MCX W23 Power Profile Tools (including Localization)

Jump to solution
17,044 Views
christophe_menard
NXP Employee
NXP Employee

This page is dedicated to the Kinetis (KW35/KW38/KW45/KW47) and MCX Wx (MCX W71/72 & MCX W23) Power Profile Tools.

It will help you to estimate the power consumption in your application (Automotive or IIoT) and evaluate the battery life time of your solution.

This page content 7 dedicated power profile tool for:

  1. Bluetooth LE for the KW35/KW38 products in standalone (Automotive).
  2. Bluetooth LE for the KW45/KW47 products in standalone (Automotive).
  3. Bluetooth LE for the MCX W71/MCX W72 product in standalone (IIoT).
  4. Bluetooth LE for the MCX W23 product in standalone (IIoT).
  5. 802.15.4 Matter ICD SIT & LIT and ZED for the MCX W71 & W72 product in standalone (IIoT).
  6. SmartFob application (BLE/KW45; UWB Ranger4; SE; motion sensor) (Automotive)
  7. Localisation application (CCCv4) (Automotive & IIoT)

 

1. KW35/KW38 Bluetooth LE power profiling for Automotive

christophe_menard_3-1758726960001.png

 

This tool includes 3 different use cases to get a rough estimation of the Anchor and Keyfob/Smartphone power consumptions:

   1- CCC mobile phone connected to the car and exchange packets to unlock the door of the car

   2- SCA Keyfob connected to the car and exchange packets continuously

   3- CCC Smartphone connected to the car and exchange packets continuously : 2 row modes

christophe_menard_6-1710781541302.png

2. KW45/KW47 Bluetooth LE power profiling for Automotive

christophe_menard_0-1758726282496.png

3. MCX W71 / MCX W72 Bluetooth LE power profiling for IIoT

christophe_menard_0-1719240520534.png

4. MCX W23 Bluetooth LE power profiling for IIoT

christophe_menard_1-1758726727635.png

 

5. 802.15.4 Matter ICD SIT & LIT and ZED MCX W71/W72 Power profiling

christophe_menard_0-1757492591715.png

 

6. Smartfob (BLE+UWB) Power profiling

christophe_menard_4-1710780975560.png

 

7. KW47 CCC CS localization power profile

2 automotive applications example are available in the KW47 SDK:

...\kw47b41zevk\wireless_examples\bluetooth\digital_key_car_anchor_cs

...\kw47b41zevk\wireless_examples\bluetooth\digital_key_device_cs

KW47 Digital Key CCC CS Power Estimator tool v0.10.xlsx

christophe_menard_2-1758726829231.png

2 IIoT applications example are available in the MCX W72 SDK:

...\MCX W72\boards\mcxw72w148evk\wireless_examples\bluetooth\loc_reader

...\MCX W72\boards\mcxw72w148evk\wireless_examples\bluetooth\loc_user_device

 

Please, find this important link to build a PCB using a KW45/MCX W71 or KW47/MCX W72 and all concerning the radio performances and radio certification (CE/FCC/IC):

The best way to build a PCB using a KW45 (car acce... - NXP Community

 

For Power and Low Power Application Notes please see product pages. Here are some direct links for your convenience:

MCXW71 - Power Management Hardware

MCX W71 Bluetooth LE Power Consumption Analysis

KW45/K32W148 - Power Management Hardware

Kinetis KW45 and K32W1 Bluetooth LE Power Consumption Analysis

 

0 Kudos
Reply
1 Solution
15,305 Views
christophe_menard
NXP Employee
NXP Employee

Hi Everett,

The password is in place to avoid changes or competitor benchmarks in too much details.

Sorry for the inconvenient but it can't be.

View solution in original post

2 Replies
15,306 Views
christophe_menard
NXP Employee
NXP Employee

Hi Everett,

The password is in place to avoid changes or competitor benchmarks in too much details.

Sorry for the inconvenient but it can't be.

15,337 Views
EverettRao
NXP Employee
NXP Employee

Hi  christophe_menard,

@christophe_menard  Could you provide the password of Sheet protection, thanks very much.

EverettRao_0-1729134009121.png

 

0 Kudos
Reply