KW01 UI question

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KW01 UI question

1,078件の閲覧回数
cwchen14
Contributor I

Hi, I founded an exe file named "KW01_Connectivity_Software.exe" on the official website of NXP, is that a UI used for KW01?

If the answer is not, where could I download the UI?

Does the UI use for free?     

0 件の賞賛
返信
1 返信

1,038件の閲覧回数
Sebastian_Del_Rio
NXP Employee
NXP Employee

Hi Sean, I hope you're doing well!

 

The KW01's connectivity software is a collection of different drivers and example code developed for this MCU. When executing the file, it will install the SDK and some example projects to the specified path. These projects can be opened and edited using the IAR Embedded Workbench IDE.

 

For more information, there's some documentation included in the installation directory, inside the "doc" folder, covering different topics like development process and stack explanations.

 

Please let me know if you have any further questions.

 

Best regards,

Sebastian

0 件の賞賛
返信