KINETIS: random por reset when enter VLPS mode

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

KINETIS: random por reset when enter VLPS mode

937 次查看
minli
Contributor I

code is as follows, I didn't write this code and I am unable to find out at which point does the reset happens. But it did happen during this code. Any insight? Thanks

/*
* This code runs from eSRAM (on-chip SRAM).
*/

.global kinetis_suspend_to_ram
.global kinetis_suspend_to_ram_end
.align 4

kinetis_suspend_to_ram:
push {lr}

/*
* Put DDR into self-refresh
*/
ldr r0, ddr_cr16
mov r1, #0x10000
add r1, #0x0
str r1, [r0]

ldr r0, ddr_cr15
mov r1, #0x10000
add r1, #0xF
str r1, [r0]

ldr r0, sim_mcr
ldr r1, [r0]
add r1, #0x1
str r1, [r0]

/*
* Disable all DDR I/O pins
* Disable DDR_DQS
*/
ldr r0, sim_mcr
ldr r1, [r0]
movw r2, #0xFFF3
movt r2, #0xFFFF
and r1,r2
str r1, [r0]

/*
* Disable clock to the DDR controller
*/
ldr r0, sim_scgc3
ldr r1, [r0]
movw r2, #0x0
movt r2, #0xBFFF
and r1,r2
str r1, [r0]

/*
* We switch the MCG mode from PEE all the way to BLPI.
* BLPI = PLL is disabled, FLL is disabled, clock is derived
* from the internal refernence clock.
* We need that so that on wake up from VLPS the Kinetis
* returns to BLPI, rather than automatically return to PBE,
* resetting the clocks and hence baud rates for UART, etc.
*
* Switch from PEE to PBE
*/
ldr r0, mcg_c1
ldrb r1, [r0]
orr r1, #0x80
strb r1, [r0]

/*
* Wait until CLKS has switched to PBE
*/
1:
ldr r0, mcg_s
ldrb r1, [r0]
and r1, #0x0C
cmp r1, #0x08
bne 1b

/*
* Switch from PBE to FBE
*/
ldr r0, mcg_c6
ldrb r1, [r0]
and r1, #0xBF
strb r1, [r0]

/*
* Wait until CLKS has switched to FBE
*/
1:
ldr r0, mcg_s
ldrb r1, [r0]
and r1, #0x20
cmp r1, #0x00
bne 1b

/*
* Switch from FBE to FBI
*/
ldr r0, mcg_c1
ldrb r1, [r0]
and r1, 0x3F
//orr r1, #0x46
orr r1, #0x40
strb r1, [r0]

/*
* Wait until CLKS has switched to FBI
*/
1:
ldr r0, mcg_s
ldrb r1, [r0]
and r1, #0x0C
cmp r1, #0x04
bne 1b

/*
* Switch from FBI to BLPI. Set LP
*/
ldr r0, mcg_c2
ldrb r1, [r0]
orr r1, #0x02
strb r1, [r0]

/*
* Switch to Deep Sleep
*/
dsb
isb

nop
nop
nop
nop

wfi

/*
* When at this point, we have been woken from Deep Sleep.
* Since we entered VLPS in BLPI Mode, we exit in BLPI mode as well.
*/

/*
* Switch from BLPI to FBI. Unset LP
*/
ldr r0, mcg_c2
ldrb r1, [r0]
and r1, #0xFD
strb r1, [r0]

/*
* Switch from FBI to FBE
*/
ldr r0, mcg_c1
ldrb r1, [r0]
and r1, #0x3B
orr r1, #0x82
strb r1, [r0]

/*
* Wait until reference clock has switched to external clock
*/
1:
ldr r0, mcg_s
ldrb r1, [r0]
and r1, #0x10
cmp r1, #0x10
beq 1b

/*
* Wait until CLKS has switched to FBE
*/
1:
ldr r0, mcg_s
ldrb r1, [r0]
and r1, #0x0C
cmp r1, #0x08
bne 1b

/*
* Switch from FBE to PBE
*/
ldr r0, mcg_c6
ldrb r1, [r0]
orr r1, #0x40
strb r1, [r0]

/*
* Wait until PLL1 has locked up
*/
1:
ldr r0, mcg_s2
ldrb r1, [r0]
and r1, #0x40
cmp r1, #0x40
bne 1b

/*
* Switch from PBE to PEE
*/
ldr r0, mcg_c1
ldrb r1, [r0]
and r1, #0x3F
strb r1, [r0]

/*
* Wait until CLKS switches to PEE
*/
1:
ldr r0, mcg_s
ldrb r1, [r0]
and r1, #0x0C
cmp r1, #0x0C
bne 1b

/*
* Enable all DDR I/O pins
* Enable DDR_DQS
*/
ldr r0, sim_mcr
ldr r1, [r0]
add r1, #0xC
str r1, [r0]

/*
* Enable the clock to the DDR controller
*/
ldr r0, sim_scgc3
ldr r1, [r0]
orr r1, #0x4000
str r1, [r0]

/*
* Take DDR out of self-refresh
*/
ldr r0, sim_mcr
ldr r1, [r0]
movw r2, #0xFFFE
movt r2, #0xFFFF
and r1,r2
str r1, [r0]

ldr r0, ddr_cr15
mov r1, #0xF
str r1, [r0]

nop
nop
nop
nop

/*
* Return to the kernel code running from DDR
*/
pop {pc}
bx lr

.align 4
ddr_cr15 :
.word 0x400AE03C
ddr_cr16 :
.word 0x400AE040
sim_mcr:
.word 0x4004806C
sim_scgc3:
.word 0x40048030
mcg_c1:
.word 0x40064000
mcg_c2:
.word 0x40064001
mcg_c6:
.word 0x40064005
mcg_s:
.word 0x40064006
mcg_s2:
.word 0x40064012

.align 4
kinetis_suspend_to_ram_end:
.word 0

0 项奖励
回复
0 回复数