K32W061/JN5189: Thread support for ‘Enhanced Frame Pending' (EFP)?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

K32W061/JN5189: Thread support for ‘Enhanced Frame Pending' (EFP)?

Jump to solution
573 Views
ckielstra
Contributor II

Which version of Thread is supported by the current NXP SDK (v2.6.13)?

I'm asking because we want to use the Enhanced Frame Pending (EFP) feature introduced in Thread v1.2.
If already supported by the SDK, then how do we activate this feature?

0 Kudos
Reply
1 Solution
550 Views
Ricardo_Zamora
NXP TechSupport
NXP TechSupport

Hello,

 

Hope you are doing well. The OpenThread middleware is not included on the SDK. You need to get it from the GitHub - NXP/ot-nxp: OpenThread on NXP examples.

 

Please check the information of each release directly: Releases · NXP/ot-nxp · GitHub

 

Regards,

Ricardo

View solution in original post

0 Kudos
Reply
1 Reply
551 Views
Ricardo_Zamora
NXP TechSupport
NXP TechSupport

Hello,

 

Hope you are doing well. The OpenThread middleware is not included on the SDK. You need to get it from the GitHub - NXP/ot-nxp: OpenThread on NXP examples.

 

Please check the information of each release directly: Releases · NXP/ot-nxp · GitHub

 

Regards,

Ricardo

0 Kudos
Reply