Jtagkey debug JN5168

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Jtagkey debug JN5168

3,314件の閲覧回数
darlington
Contributor I

Dear Ms, Mr,

I'm developing a project on a JN5168 and I'd like to debug it with the Amontec JtagKey 2 but I have this issue when I launch the debug mode:

(JN-AN-1174 project)

jp3: JTAG protocol via USB/parallel port for Windows.

Version 1.6.3

Assuming debug_if's TAP has an IDCODE of 0x14951185.

Using 'Amontec Amontec JTAGkey-2 (556XNII6)' interface.

Enabling high speed ftdi mode.

Using JTAG clock of 15 MHz

Enabling UART not supported/required on this adapter.

In my makefile, I have:

DEBUG ?=HW

DEBUG_PORT ?= UART0

and TRACE ?=1

I respected the application note to start the debug (debug configuration -> _hwdbg.elf ...)

And I also have the transistor on a special pin like this :

P1000880.jpg

Can we debug on the JN5168? If yes, what could be my mistake?

Thank you!

タグ(3)
0 件の賞賛
返信
3 返答(返信)

2,899件の閲覧回数
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Guillaume,

JTAG Debug is supported on the JN516x series of devices when using the latest JN-SW-4141 BeyondStduion for NXP

Could you take a look of this application note which provides a step-by-step guide

http://www.nxp.com/documents/application_note/JN-AN-1203.pdf

Let me know if you still have problems with the debug

Best Regards

Mario

0 件の賞賛
返信

2,899件の閲覧回数
darlington
Contributor I

Hello Mario,

Thank you for your answer.

I did it but I always got this error message (on my first post). I don't have the carrier and the expension board but my JN5168 works and I made a DIY expension board with the schematic on my first post (the same as yours thanks to the DR1222_Schematic_1V2 document).

have you got any idea?

Best regards,

Guillaume

0 件の賞賛
返信

2,899件の閲覧回数
billkrakar
NXP Employee
NXP Employee

Hi Guillaume

NXP Technical Information Center (TIC) has been notified to dispatch this request.

Please advise if you don't get a response in the next couple of days.

Thanks!

Bill Krakar

0 件の賞賛
返信