JN5189 jn5189dk6_zigbee_ed_rx_on_bm is working only in debugging mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

JN5189 jn5189dk6_zigbee_ed_rx_on_bm is working only in debugging mode

1,508件の閲覧回数
devaiah
Contributor II

I am working with JN5189 DK6 board and trying to compile and run the SDK example "jn5189dk6_zigbee_ed_rx_on_bm". The problem I am facing is that it is working fine in Debug mode with debugger attached but the moment the debugger is plugged out the reset of the board is done it simply stops working I do not even see any debug prints on UART0 line as well.

Below are my IDE & SDK versions:

MCUXpresso IDE Version: MCUXpresso IDE v11.3.1 [Build 5262]

SDK Version: 2.6.3(464 2021-04-08).

Hoping to get a prompt response.

 

Regards,

Devaiah

 

ラベル(2)
0 件の賞賛
返信
1 返信

1,493件の閲覧回数
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi @devaiah,

I hope you are doing great.

Please look at the JN-AN-1260 that describes the setup that you need JN5189/88.

Let me know if you are still facing this issue.

Regards,

Mario

0 件の賞賛
返信