JN5168 transmission and reception issue,how to set continuous wave??,Measure LQI in dBm??

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

JN5168 transmission and reception issue,how to set continuous wave??,Measure LQI in dBm??

1,432件の閲覧回数
shaileshkorat
Contributor I

1. I am working on communication between 2 JN5168 modules. When i send

   data from one module to another , receiver receives data successfully.

   But after few days , receiver module stops receiving any data. Firmware

   on both device is same. When i used sniffer , i can see packets from

   sender in both cases. So , transmission is not an issue. Is their any

   possibility that RF receiver stops working in JN5168?

2. how to set jn5168 in CW(continuous wave) mode?

3. How to represent LQI in dBm?

タグ(3)
0 件の賞賛
返信
1 返信

1,074件の閲覧回数
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi,

Please look at the  Application Note: JN-AN-1172. The example provides a CW using the terminal, you could look at the implementation.

Look at the Transmit Power Test (CW Mode)

The CW mode Transmit Power Test puts the device into a transmit state, generating a continuous wave signal.

Regards,

Mario

0 件の賞賛
返信