JN5168-How many nodes can be connected by one Co-ordinator

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

JN5168-How many nodes can be connected by one Co-ordinator

ソリューションへジャンプ
1,873件の閲覧回数
xubovey
Contributor III

hi,

in my application, i used the JN5168-001-MXX, and there was only one Co-ordinator and 100 End devices, without Routers.

question was the parm Child Table Size in Network layer Configturation could not be bigger than 48. i donot know why.

was there anyway to solve my problem. thanks a lot.

i used the JN-AN-1229.

タグ(1)
0 件の賞賛
返信
1 解決策
1,710件の閲覧回数
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi,

Remember the JN5168-001-MXX has some memory size Flash 64/160/256K, so when you are join more than 48 devices, you are exceed the memory.

But, you can try with the IEEE 802.15.4 for JN516x and JN517x|NXP, if your application doesn't required Zigbee protocol.

Best Regards,

Mario

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,711件の閲覧回数
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi,

Remember the JN5168-001-MXX has some memory size Flash 64/160/256K, so when you are join more than 48 devices, you are exceed the memory.

But, you can try with the IEEE 802.15.4 for JN516x and JN517x|NXP, if your application doesn't required Zigbee protocol.

Best Regards,

Mario

0 件の賞賛
返信
1,710件の閲覧回数
xubovey
Contributor III

Hi

thanks a lot for your reply.

i have found JN-AN-1069,and it works very well.

0 件の賞賛
返信