JN5161 can't control actuator with security level 2

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

JN5161 can't control actuator with security level 2

1,187 Views
26803385
Contributor I

Hi Sir:

Now I am using JN5161, and using AN1219 (v1007) to develop a Zigbee green power switch..

I found a strange problem.. 

When i using security level 3, means  "GPD_SECURITY_LEVEL_FC_4B_MIC_4B_WITH_ENC", and the actuator designed by Silabs MG21 can receive the commissioning and toggle telegram send from switch.

But when i using security level 2, means "GPD_SECURITY_LEVEL_FC_4B_MIC_4B_NO_ENC", the same actuator can only receive commissioning telegram, and have no response with toggle telegram.

I guess MG21 ignored the toggle telegram because something is wrong..

 

The question is why it happens? Thanks.

Labels (2)
0 Kudos
Reply
1 Reply

1,149 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Zero,

Do you have the sniffer log about this issue?

Where are you changing the security level?

Could you please provide more information about this issue?

Regards,

Mario

0 Kudos
Reply