Is there a way to restart Co-ordinator in such a way that remote nodes do not need to re-enter the network?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Is there a way to restart Co-ordinator in such a way that remote nodes do not need to re-enter the network?

1,139 次查看
xleaderx
Contributor I

Hello guys!
I have a question.
I'm using the ZigBee JN5168 module in our project.
My software uses the JN-SW-4170 SDK.
The software is based on the example JN-AN-1229-ZBPro-Application-Template using the ZBPro stack.

I often have situations when it is necessary to restart the Co-ordinator without restarting the entire ZigBee network.
But, in this case, it is no longer possible to communicate with the remote nodes.
Communication is restored only when the nodes re-enter the network.

Is there a way to restart Co-ordinator in such a way that remote nodes do not need to re-enter the network?

标签 (3)
0 项奖励
回复
1 回复

1,094 次查看
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi,

By default, the JN-AN-1229 is not saving the Zigbee network information. That is the reason for the devices need to join a new network. You could take a look to the JN-AN-1217 and look t the save process.

Regards,

Mario

0 项奖励
回复