Is the optimal channel and device on line?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is the optimal channel and device on line?

1,367件の閲覧回数
LChll
Contributor III

I am developing some 3.0 devices with JN5169, the SDK is jn-sw-4170.

1、Can the coordinator automatically select the optimal channel for network construction?Routine 1216 should be a random channel.

2、How does the gateway determine if a device (router or enddevice) is online?

ad
ラベル(2)
0 件の賞賛
返信
1 返信

1,292件の閲覧回数
Sebastian_Del_Rio
NXP Employee
NXP Employee

Hi Linklai, I hope you're doing well!

 

  1. As a part of both, the ZigBee 3.0 and IEEE802.15.4, a process called Clear Channel Assessment (or CCA) is performed during the network creating steps to determine which channel is best for the network to be started on. This process is performed automatically.
  2. The gateway device can send an Active Request to a specific device by using its short address to determine if it is currently powered and connected to the network.

 

Please let me know if you need any further information.

 

Best regards,

Sebastian

0 件の賞賛
返信